Technical FAQs

Ask a Question

Will a HOM2030M150TC load center accept a HOMT tandem or quad tandem circuit breaker?

Yes, this is a 20 space/30 circuit panel, accepting a maximum of (10) HOMT tandem or (4) HOMT quad tandem circuit breakers.

CTA-ID : 2002269
Was this helpful?
What can we do to improve the information ?