Technical FAQs

Ask a Question

Will a HOM1624L125C load center accept a HOMT tandem or quad tandem circuit breaker?

Yes, this is a 16 space/24 circuit panel, accepting a maximum of (8) HOMT tandem or (4) HOMT quad tandem circuit breakers.


CTA-ID : 2002267
Was this helpful?
What can we do to improve the information ?