Technical FAQs

Ask a Question

Will a HOM1632U200TC load center accept a HOMT tandem or quad tandem circuit breaker?

Yes, this is a 16 space/32 circuit panel, accepting a maximum of (16) HOMT tandem or (8) HOMT quad tandem circuit breakers.

CTA-ID : 2002266
Was this helpful?
What can we do to improve the information ?