Technical FAQs

Ask a Question

Will a HOM2040M200RB load center accept a HOMT tandem or quad tandem circuit breaker?

Yes, this is a 20 space/40 circuit panel, accepting a maximum of (20) HOMT tandem or (10) HOMT quad tandem circuit breakers.

CTA-ID : 2002254
Was this helpful?
What can we do to improve the information ?