Technical FAQs

Ask a Question

What wire sizes are recommended for Modular and Non-Modular TVSS devices?

XGA terminals will accept #12 to #6 AWG copper wire for phase, neutral and ground conductors. Torque connections to 50 lb-in for devices without a circuit isolator and 15 lb-in. for devices with a circuit isolator.

XF/XP terminals will accept #12 to #8 AWG copper wire for phase, neutral and ground connectors. Torque connections to 18 lb-in.




CTA-ID : 2002032
Was this helpful?
What can we do to improve the information ?