Technical FAQs

Ask a Question

What are the dimensions of the HOMC20U100C load center cover?

Issue:
Dimensions

Product Line:
QO Load Center

Environment:
Dimensions

Cause:
Dimensions

Resolution:

This cover is approximately 27.24" H x 15.44" W. The cover will overlap the load center enclosure by approximately 0.60" (19/32``) on all sides.


CTA-ID : 2001755
Was this helpful?
What can we do to improve the information ?