Technical FAQs

Ask a Question

Since the FY breakers are no longer available in panelboards, are the FD, FG, and FJ breakers able to be used as a switch duty breaker?

Yes. If this is being questioned by the customer or inspector, the faceplate of the breaker indicates it can be used in a switch duty application in a panelboard.

CTA-ID : 2002482
Was this helpful?
What can we do to improve the information ?