Technical FAQs

Ask a Question

Will a HOM1224M125TC load center accept a HOMT tandem or quad tandem circuit breaker?

Yes, this is a 12 space/24 circuit panel, accepting a maximum of (12) HOMT tandem or (6) HOMT quad tandem circuit breakers.


CTA-ID : 2002252
Was this helpful?
What can we do to improve the information ?