Technical FAQs

Ask a Question

Will a HOM816M200FTRB load center accept a HOMT tandem or quad tandem circuit breaker?

Yes, this is a 8 space/16 circuit panel, accepting a maximum of (8) HOMT tandem or (4) HOMT quad tandem circuit breakers.


CTA-ID : 2002242
Was this helpful?
What can we do to improve the information ?