Technical FAQs

Ask a Question

Will a HOM816L125C load center accept a HOMT tandem or quad tandem circuit breaker?

Yes, this is a 8 space/16 circuit panel, accepting a maximum of (8) HOMT tandem or (4) HOMT quad tandem circuit breakers.

CTA-ID : 2002244
Was this helpful?
What can we do to improve the information ?