Technical FAQs

Ask a Question

What is the Terminal Lug Data for the HU365DS and HU365AWK, Series E2 Heavy Duty safety switch?

Issue:
Product features

Product Line:
HD Safety Switch

Environment:
Lug wire size

Cause:
Installation

Resolution:
The lugs on this switch will accept (1) #1 AWG - 600 kcmil or (2) #1 AWG - 250 kcmil copper conductors per phase.


CTA-ID : 2001494
Was this helpful?
What can we do to improve the information ?