Technical FAQs

Ask a Question

How much force does it take to toggle the handle of an NA or NC breaker?

From Off to On it takes 50 lbs of force
From On to Off it takes 15 lbs of force
From trip to reset it takes 45 lbs of force

CTA-ID : 2001488
Was this helpful?
What can we do to improve the information ?