Technical FAQs

Ask a Question

How many neutral and ground terminations are there in a QOM22225NS circuit breaker enclosure?

There are two neutral lugs (1 incoming - 1 outgoing) suitable for #4 AWG - 250 kcmil aluminum or copper conductors. There are four service grounding lugs factory installed on the neutral assy, for Service Equipment applications, each suitable for #12 - 2/0 AWG aluminum or #14 - 2/0 AWG copper conductors. For other applications, a PKOGTA2 equipment ground kit is factory included, but not installed. This kit consists of two lugs, suitable for #6 - 2/0 aluminum or #10-2/0 copper conductors.


CTA-ID : 2001238
Was this helpful?
What can we do to improve the information ?