Technical FAQs

Ask a Question

Is there a master password for the Omegapak 8804 Digital Operator Interface? What can a user do if they forget a password they entered?

The master password is 10161 & this can be used to over write any other password that was enter.  The master password can not be modified.

If a user forgot their password, when making a change and prompted by the keypad, enter the master password.

The user should immediately proceed to Menu 2, sub-menu 1 (to modify) or 2  (disable the password) before forgetting to make any other change.

Refer to bulletin 50006-377-02A, page 41 & 42, for more details.

(Related to resolution 4070)

CTA-ID : 4123
Was this helpful?
What can we do to improve the information ?