Technical FAQs

Ask a Question

What is the adjustment range for the adjustable length lever arm on an XCKT145?

The minimum length is 1.5``; the maximum length is 3.25`` as measured from the center of the pivot point out to the top edge of the roller.

CTA-ID : 2000740
Was this helpful?
What can we do to improve the information ?