Technical FAQs

Ask a Question

What is the Terminal Lug Data for a HU265, Series E2 Heavy Duty safety switch?

The lugs on this device will accept (1) #1/0 AWG - 750 kcmil or (2) #1/0 AWG - 300 kcmil aluminum or copper conductors per phase.


CTA-ID : 2001466
Was this helpful?
What can we do to improve the information ?