Technical FAQs

Ask a Question

Can the cover of a QO2100BNS surface mount circuit breaker enclosure be changed to adapt the enclosure to a flush mount application?

No. Although the cover of the QO2100BNF (flush mount) will physically fit onto the QO2100BNS enclosure, we do not recommend this conversion by merely replacing the cover. Replacement covers do not have nameplates or labels applied to them. If a new QO2100BNF were purchased, its cover would physically be able to be placed onto the QO2100BNS enclosure and it would have the appropriate labeling and nameplate.


CTA-ID : 2001230
Was this helpful?
What can we do to improve the information ?