Technical FAQs

Ask a Question

How does the contact arrangement on a 9001 KR8*H25 work?

The H25 consists of a 9001 KA5, which will be closed in the center and the pulled positions, and a 9001 KA3, which will be closed in the pulled position and open in the center position. They are both open in the pushed position configuration contacts sequencing

CTA-ID : 13488
Was this helpful?
What can we do to improve the information ?