Technical FAQs

Ask a Question

Is R2 relay programmable on the ATV28?

Issue:  Is R2 relay programmable on the ATV28?
 
Product Line:  ATV28
 
Environment:  All
 
Cause:  N/A
 
Resolution:  Yes.


 
Was this helpful?
What can we do to improve the information ?