Technical FAQs

Ask a Question

Can the main breaker in a HOM20M100RB load center be changed to 125 ampere?

No, the main breaker ampere rating cannot exceed the ampere rating of the panel. The HOM20M100RB is listed and labeled as a 100 ampere rated panel. The main breaker, therefore, could not exceed 100 ampere.


CTA-ID : 2000725
Was this helpful?
What can we do to improve the information ?