Technical FAQs

Ask a Question

What is the Terminal Lug Data for the HU365R, HU365, HU365AWK, HU365DS, Series E2 Heavy Duty safety switches?

Issue:
Product features

Product Line:
HD Safety Switch

Environment:
Lug wire size

Cause:
Installation

Resolution:
The lugs on these Series E2 switches, will accept (1) #1/0 AWG - 750 kcmil or (2) #1/0 AWG - 300 kcmil aluminum or copper conductors per phase.


CTA-ID : 2001468
Was this helpful?
What can we do to improve the information ?