Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H265R, Series E2 Heavy Duty safety switch?

Issue:
Product Features

Product Line:
Heavy Duty Safety Switches

Environment:
Main lug wire range

Cause:
Installation

Resolution:
The lugs on this device will accept (1) #1/0 AWG - 750 kcmil or (2) #1/0 AWG - 300 kcmil aluminum or copper conductors per phase.

 
Was this helpful?
What can we do to improve the information ?