Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H365R, Series E2 Heavy Duty safety switch?

Issue:
Product design features

Product Line:
Heavy Duty Safety Swithces

Environment:
Main lug wire sizes

Cause:
Application

Resolution:
The lugs on this device will accept (1) #1/0 AWG - 750 kcmil or (2) #1/0 AWG - 300 kcmil aluminum or copper conductors per phase.


CTA-ID : 2001463
Was this helpful?
What can we do to improve the information ?