Technical FAQs

Ask a Question

What is maximum load for the 24 volt power supply on ATV58?

The +24 can provide up to 200mA. It is protected against short circuit.
Each Logic input uses about 7 mA.


CTA-ID : 2001212
Was this helpful?
What can we do to improve the information ?