Technical FAQs

Ask a Question

Is an Underground Service Wireway available for the MP metering devices?

Yes, the Underground Service Wireway products were introduced in February, 2002. These UG Service Wireway products are not load-bearing; they are intended for use only as a means to cover and secure service entrance cables prior to entering a wall mounted MP METER-PAK device. For selection, please refer to the document link provided below for the Residential Products Catalog. Refer to the Table of Contents for the Metering section.

CTA-ID : 2001066
Was this helpful?
What can we do to improve the information ?