Technical FAQs

Ask a Question

What is the lug temperature rating for an 9080 LB power distribution blocks?

Lugs are suitable for use with 75 degree rated conductors.


CTA-ID : 2000974
Was this helpful?
What can we do to improve the information ?