Technical FAQs

Ask a Question

What is the magnetic (instantaneous) multiplier to determine the equivalent DC trip range for the LA/LH ac breaker?

The multiplier is 1.2 for the high setting, 1.4 for the low setting.   See data bulletin 0100DB0101 for complete details on rerating for direct current.


CTA-ID : 2000953
Was this helpful?
What can we do to improve the information ?