Technical FAQs

Ask a Question

Is the FSP260 the same size as the FSP230?

Product Features

Product Line:
Obsolete AC Disconnects

Dimension clarification

The FSP260 and the FSP230 bases are different in size. The difference is the ampere rating and the size of fuses used.
These units are obsolete and no longer offered. 

CTA-ID : 2001439
Was this helpful?
What can we do to improve the information ?