Technical FAQs

Ask a Question

What is the horsepower rating of a HU664DS safety switch?

This switch is rated for 60 HP @ 240Vac, 3-phase, 125 HP @ 480Vac, 3-phase or 150 HP @ 600Vac, 3-phase. The HP ratings applicable for a safety switch are printed on the Wiring Diagram, located inside the front cover of the switch.


CTA-ID : 2001436
Was this helpful?
What can we do to improve the information ?