Technical FAQs

Ask a Question

What is the coil burden for a 1021 shunt trip suffix?

It is 24VA at 120V, 107VA at 208V, 154VA at 240V


CTA-ID : 2001178
Was this helpful?
What can we do to improve the information ?