Technical FAQs

Ask a Question

What is the part number for an 18`` rail extension assembly for NF panelboards?

The part number for the 18`` rail extension assembly is 80113-115-52. These extensions must mount on the end opposite the main. They are not available with sub feed breakers, feed-thru lugs, split bus, or column width interiors. This part number does not include a deadfront extension.


Revised 3/2/04



CTA-ID : 2001420
Was this helpful?
What can we do to improve the information ?