Technical FAQs

Ask a Question

Can the HOM1224L125TC load center be converted to a Main Breaker load center?

Product design features

Product line:
Homeline load centers

Convert to main breaker



The answer is dependent upon the Series number of the HOM1224L125TC. Series 2 and Series 3 were considered "fixed Main Lugs" and not convertible to Main Breaker. A Series S01 or S03 device may be converted to a Main Breaker by using a QOM50VH (50 amp) through QOM125VH (125 amp) Main Circuit Breaker Kit. A QOM125VH would be the maximum Main Breaker allowed.

CTA-ID : 2001415
Was this helpful?
What can we do to improve the information ?