Technical FAQs

Ask a Question

What is the part number for replacement fuse clips for the QMB363T31?

QMB363T31W, Series E1. This is a double unit with a; 100amp on one side and 30amp on the other.
Fuse clips are not replaceable by themselves.
Line Base Assys are not replaceable.

100 amp - Load Base Assy is; 40520-216-50.
30 amp - Load Base Assy is; 40520-207-50.




CTA-ID : 2001159
Was this helpful?
What can we do to improve the information ?