Technical FAQs

Ask a Question

What Class R Fuse Kit is used with the H322N safety switch?

Issue:
Selection

Product Line:
HD SS

Cause:
Accessory Selection

Resolution:
The correct kit is dependent upon the Series number of the switch. For Series E1, use HRK60. For Series F1 or F3, use RFK06. For Series F4 or F5, use RFK03H.
For othe Series Numbers, please contact 1-888-778-2733, Opt. 1, Opt. 1, Opt. 4.



CTA-ID : 2001157
Was this helpful?
What can we do to improve the information ?