Technical FAQs

Ask a Question

Why doesn't a ZB4BW553 and a ZB4BW061 fit together?

Issue:
Why doesn't a ZB4BW553 and a ZB4BW061 fit together?

Product Line:
Harmony Pushbuttons

Environment:
All Products

Cause:
Product Features

Resolution:
The ZB4BW553 are for use with protected LED light modules only. The ZB4BW061 uses a BA9 base lamp and will not fit in the ZB4BW553. Suggested they change operator to a ZB4BW33 and use boot ZB4PO or ZB4P0A for food industry applications.


CTA-ID : 2000949
Was this helpful?
What can we do to improve the information ?