Technical FAQs

Ask a Question

Is a NEMA 1 enclosure available for the QOM2 circuit breaker?

Yes, use QOM22225NS for a NEMA 1 surface mount application. Use QOM22225NF for a NEMA 1 flush mount application. Use QOM22225NRB for a NEMA 3R application. No other NEMA type enclosures are available for the QOM2 circuit breaker.


CTA-ID : 2000664
Was this helpful?
What can we do to improve the information ?