Technical FAQs

Ask a Question

What are the rail and deadfront extensions required to mount an NF430L2 or NF430L2C in an MH50?

The following parts will be required per panel and can only be installed opposite the mains end:

(1) 80113-115-51 12`` rail extension kit
(1) 80113-175-54 12`` ext load end cover





CTA-ID : 2001150
Was this helpful?
What can we do to improve the information ?