Technical FAQs

Ask a Question

Can a mushroom button be installed on the 9001 KR11UH1 interlocked buttons?

There are no provisions for this. The snap in mushroom button has a locating nib on it to keep it from rotating and there is no corresponding hole for it to fit in on the grey cap on the KR11U. This nib can be cut off, but is not recommended. Suggest they can order the 9001 KR11UG22 or KR11UR22 to get unit with mushroom button.


CTA-ID : 2001146
Was this helpful?
What can we do to improve the information ?