Technical FAQs

Ask a Question

Do I-line breakers come with the tin piece that is on the back end of the breaker and is screwed into panel?

Mounting bracket is integral part of each I-Line circuit breaker and securely supports and aligns load end of breaker.

CTA-ID : 2001144
Was this helpful?
What can we do to improve the information ?