Technical FAQs

Ask a Question

Can a H361 be used on 125Vdc, 250Vdc, as well as 600Vdc?

Yes. It is rated up to 600Vdc maximum.


CTA-ID : 2000915
Was this helpful?
What can we do to improve the information ?