Technical FAQs

Ask a Question

What is the voltage rating for the 92351Double Throw safety switch?

The 92351 is rated for up to 240Vac or 250Vdc maximum.


CTA-ID : 2000637
Was this helpful?
What can we do to improve the information ?