Technical FAQs

Ask a Question

Did the catalog number QON442MS300 come with an enclosure and cover?

Issue:
Product Design Features

Product Line:
QO Load centers

Environment:
Enclosure and Cover

Cause:
Selection

Resolution:
The QON442MS300 was only a load center interior, the enclosure and cover were purchased separately, BUT this is an old Obsolete catalog number, SEE THE CURRENT DIGEST FOR CURRENT CATALOG NUMBERS

 
Was this helpful?
What can we do to improve the information ?