Technical FAQs

Ask a Question

What is the part number for the signal converter used on Econoflex with Modification J09 to allow 0-10 VDC speed input instead of the standard 4-20 mA source?

The part number is 3115829750.
Some documentation may show the old part number of 883910VAI. It is not a valid part number.

CTA-ID : 14417
Was this helpful?
What can we do to improve the information ?