Technical FAQs

Ask a Question

How many terminals are supplied on a SN100FA?

There are two neutral lugs (1 incoming/1 outgoing) suitable for (1) #14-1/0 AWG Copper or (1) #12 - 1/0 AWG Aluminum. There are also two grounding terminals, for use when the enclosed circuit breaker is used in a Service Equipment application, suitable for the same wire range as the neutral lugs.


CTA-ID : 2000908
Was this helpful?
What can we do to improve the information ?