Technical FAQs

Ask a Question

Does Square D offer a 240Vac, Non-Fusible, Heavy Duty safety switch?

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Environment:
Non-Fusible rated 240Vac

Cause:
Application

Resolution:
No, Square D`s Non-Fusible Heavy Duty safety switches are offered with a 600Vac maximum rating. For a 240Vac maximum application the 600Vac switch can be used or consider a General Duty safety switch.


CTA-ID : 2000635
Was this helpful?
What can we do to improve the information ?