Technical FAQs

Ask a Question

Does the NSF250N circuit breaker have a 100% rating?

No. The NSF line of breakers are 80% rated.


CTA-ID : 2000632
Was this helpful?
What can we do to improve the information ?