Technical FAQs

Ask a Question

In some documentation, the picture shows the XALD211H29, but the listing doesn`t have the H29.

Issue:
In some documentation, the  picture shows the XALD211H29, but the listing doesn`t have the H29.

Product Line:
Harmony Control Stations

Environment:
All Products

Cause:
Product Features

Resolution:
H29 is a country code for Great Britain. It would have a metric conduit entry. For a standard 1/2 inch conduit entry for US, order a XALD211.


CTA-ID : 2001110
Was this helpful?
What can we do to improve the information ?