Technical FAQs

Ask a Question

Does a MAP, 2 pole, main breaker in an I Line panelboard need to have phasing for part of the catalog number - such as; AC, AB, etc?

Issue:
Does a MAP, 2 pole,  main breaker in an I Line panelboard need to have phasing for part of the catalog number - such as;  AC, AB, etc?

Product Line:
Panelboard.

Environment:
I line panelboard.

Cause:
Product features.

Resolution:
No phasing is not needed to order. MAP main breaker is not an I Line breaker where phasing is needed.


CTA-ID : 2001109

Was this helpful?
What can we do to improve the information ?