Technical FAQs

Ask a Question

What are the dimensions on the PQ4220G plug in unit?

16.17`` W X 22.48`` H X 11.44`` D. See Busway Systems Catalog (Class 5600) for complete dimensional information.


CTA-ID : 2000610
Was this helpful?
What can we do to improve the information ?