Technical FAQs

Ask a Question

How can one determine the correct Series Number of a new safety switch for which one wishes to specify accessories?

Refer to the on-line Digest Plus Selector. The current manufacture Series Number is provided on the ``Application Data and Dimensions`` pages, next to the device catalog number in the Dimensions table. If the safety switch is already purchased, see the carton label or wiring diagram of the switch for Series Number.


CTA-ID : 2000607
Was this helpful?
What can we do to improve the information ?